Next-generation VR technology improves end effector production accuracy and speed

Auburn Hills, MI (March 29, 2017) – DESTACO, the industry’s leading global provider of high-performance automation, workholding and containment solutions, is proud to announce the launch of its new Accelerate® Vision Virtual Reality (VR) digital design solutions tool. The Accelerate Vision VR tool will be on display for attendees in Booth No. 1436 at the upcoming Automate 2017 Trade Show, which will be held from April 3-6, 2017, at McCormick Place in Chicago, IL.

Taking advantage of the latest advances in VR technology, the Accelerate Vision tool has been designed to work in the production of DESTACO’s Accelerate® Collection end effector components, which can be assembled into custom solutions for most pressroom stamping applications.

As the speed of manufacturing continues to increase, the design process for these components must also be accelerated while meeting strict demands regarding die-making and tooling accuracy and precision. By utilizing the Accelerate Vision VR digital design tool at the beginning of the design process, DESTACO is able to precisely build an end effector based on customer-supplied models and also provide detailed information and data to die-makers. This enables the die-makers to streamline their design and review process. The result is tooling that is accurate with an overall improvement in product quality for the end-user.

“Upon design review, the Accelerate Vision VR tool allows us to create complete process simulations,” explained Stefan Eggers, DESTACO’s Vice President, Global Sales & Service. “This key analysis and simulation enables us to capture interface positioning, additional collision points and maximize the press speed. After detailed simulation analysis is verified, we can move to accurately build and validate the end effector tool.”

The Accelerate Vision VR tool is part of DESTACO’s suite of Accelerate® Digital Solutions, which also includes simulation and manufacturing components. These Digital Solutions also allow the use of robot-assisted production cells during manufacturing operations, with the robot possessing the capability to increase the precision in which parts are built without the need for samples or 2D drawings. Once the construction of the component is complete, it goes through a laser-validation process to confirm that all measurements are in compliance with the approved design.

For more information about DESTACO’s Accelerate® Digital Solutions, please visit the webpage or contact DESTACO's experts.

点击此处获取客户支持

As a Global company, DESTACO has customer service representatives based in your region, no matter where you are in the world. Contact DESTACO Customer Service in your region for technical assistance, repairs, field service and more

打电话给我们 ()