Destaco Logo
News image: Introducing the New 8051 and 8331 Series Pneumatic Pull Action Latch Clamps from DESTACO

Introducing the New 8051 and 8331 Series Pneumatic Pull Action Latch Clamps from DESTACO

Introducing the New 8051 and 8331 Series Pneumatic Pull Action Latch Clamps from DESTACO

8051 and 8331 Series Pneumatic Pull Action Latch Clamps

07/23/2024 | Tags: Press Releases & News Articles - Global
News article image: Introducing the New 8051 and 8331 Series Pneumatic Pull Action Latch Clamps from DESTACO
Auburn Hills, MI, USA (07/23/2024)

DESTACO, a global leader in industrial automation, has announced the launch of the patented 8051 and 8331 Series Pneumatic Pull Action Latch Clamps. These innovative latch clamps are designed to provide superior performance and versatility for various applications in the manufacturing industry and are only offered as a standard product by DESTACO.

A key feature of the 8051 and 8331 Series Pneumatic Latch Clamps is allowing for sensors to monitor open and close positions. With 2 port options of 1/8” G or 1/8” NPT, these latch clamps offer a holding capacity of up to 600lbs (2669N) on the 8051 Series and 450lbs (2002N) on the 8331 Series, catering to a wide range of applications.

"We are proud to bring the 8051 and 8331 Series Pneumatic Latch Clamps to market, fulfilling the requests and needs of our customers," said Jeff Mruzik, Global Engineering Director at DESTACO. "These latch clamps have been highly anticipated and were previously offered as a special product. Now, we are thrilled to make them available as standard products, showcasing DESTACO's commitment to innovation and customer-centric solutions."

Designed for applications in molding, assembly, and closures, these pneumatic clamps provide unmatched performance. Featuring two cylinder bores of 20mm on the 8331 Series and 32mm on the 8051 Series, these clamps accommodate both round and square proximity sensors to monitor open or closed positions.

Customers have the option to enhance their latch clamps with optional accessories, such as specific sensors and handles, to further optimize their production processes. The versatility of the latch clamps is extended with the availability of the 8051-E, 8051-EH, 8331-E, and 8331-EH models, designed with different handle configurations and port options.

One of the unique benefits of the 8051 and 8331 Series Pneumatic Latch Clamps is the optional handle for manual positioning (-H, -EH). This handle allows operators to manually place the J-hook and secure it, with the pneumatic cylinder automatically opening it.

The sensor-ready features of the 8051 and 8331 Series Pneumatic Latch Clamps enhance their functionality, making them the first latch clamps in the market with the ability to monitor open and close positions.

DESTACO understands the importance of pressure specifications, and the 8051 and 8331 Series Pneumatic Latch Clamps have a max operating pressure of 8.3 bar [120 psi] and a min operating pressure of 2.8 bar [40 psi]. These clamps can withstand temperatures ranging from -23°C (-10°F) to 66°C (150°F) providing reliable performance in various environments.

These pneumatic latch clamps are backed by DESTACO's reputation for delivering high-quality and reliable solutions. With their secure toggle locking action, simple set-up and adjustment, and the ability to move and stay safely out of the way, these latch clamps offer the perfect solution for molding, closures for doors, lids, and covers, as well as assembly applications.

For more information about the 8051 and 8331 Series Pneumatic Pull Action Latch Clamps, please visit https://www.destaco.com/clamping/Pneumatic/Pneumatic-Toggle-Clamp/Pneumatic-Toggle-Clamp-8051-8331.html