Destaco Logo

Manual Clamping

Heavy Duty Manual Pin Package

HEAVY-DUTY MANUAL PIN PACKAGE

HEAVY-DUTY MANUAL PIN PACKAGE

DESTACO Pin Locator Clamps are primarily used in the automotive industry as a precision locating device to locate sheet metal parts for weld assembly. The pin locator units can have various attachments that are used for part location. One attachment is an NAAMS pin that is inserted into the arm that extends and retracts from the unit. This pin locates a datum hole in the part to constrain the part.