Click the magnifiying glass to search this FAQ by topic, product, or question  -

Are storage racks available?

Contact us to discuss your specific requirements as many storage racks need to be tailored to the application.

Are tool changers available in imperial and metric porting?

Yes.

Are tool changers available in stainless steel?

Yes. Contact us to discuss your specific application environment requirements.

Are tool changers for robots only?

No. Tool changers can be used anywhere that precision, rigid coupling of two components is required.

Can a tool changer be opened manually?

No, air pressure must be applied to the tool changer to separate the two halves from one another.

Can I swap out utility modules?

Yes, tool changers have a common mounting pattern for utility modules. They can easily be changed in the field when retooling your robot.

Do tool changers have failsafe features?

Yes. A spring in the piston keeps the tool changer locked securely even with loss of air pressure.

Do tool changers have standard ISO mounting?

Tool changers do follow the ISO standard, however many robot manufacturers have mounting with slight variations to this standard. Adaptors are available.

Does the ARV Venturi have a ‘Vacuum Lock’ feature?

No.

How are the utilities mounted to the tool changer?

Utilities are modular, mounting to the sides of the tool changer robot half and tool half.

How many air lines are required to operate a TPLP magnet?

One compressed air line. The magnet is free floating and will engage the part and the air line is used to release it.

If air is leaking from the tool changer, could the possible cause be that the tool changer is broken?

Yes - consult Destaco's customer service for warranty status, repair kits, or Destaco factory repair options.

If air is leaking from the tool changer, could the possible cause be that the tool changer requires maintenance?

Yes - consult the catalog maintenance section for seal kits, repair instructions, and diagrams. Contact us if the maintenance section that came with your product isn't available.

If air is leaking from the tool changer, could the possible cause be worn seals?

Yes. 1. Remove the air lines from one port and pressurize the other. The seals are worn if air comes out of the open port. 2. Seal kits are available from the accessories section of the main catalog. Most tool changers are field repairable.

If the robot will not uncouple from the tool changer, could the possible cause be a broken sensor?

Yes. 1. Check for broken sensor wires. 2. Check that the sensor is plugged into the sensor cable properly.

If the robot will not uncouple from the tool changer, could the possible cause be a collision with another object?

Yes - check for evidence of a collision involving the tool changer.

If the robot will not uncouple from the tool changer, could the possible cause be a defective valve?

Yes - check to see whether the tool changer can be actuated with a separate shop air line.

If the robot will not uncouple from the tool changer, could the possible cause be errors in the PLC program?

Yes - review the PLC program.

If the robot will not uncouple from the tool changer, could the possible cause be that debris is present in the interface?

Yes - clean all connecting surfaces, alignment pins, and sensor faces.

If the robot will not uncouple from the tool changer, could the possible cause be that the model is a faulty, spring loaded tool changer?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air lines. 2. Review the PLC program.

If the robot will not uncouple from the tool changer, could the possible cause be that the pressurized air system is contaminated?

Yes. 1. Look for particulate or water in the air lines. 2. Check that the air filter is clean.

If the robot will not uncouple from the tool changer, could the possible cause be that the tool changer is broken?

Yes - consult Destaco's customer service for warranty status, repair kits, or Destaco factory repair options.

If the robot will not uncouple from the tool changer, could the possible cause be that the tool changer mechanism is contaminated?

Yes. 1. Inspect any openings in the tool changer to see whether particulate or debris has entered the tool changer. 2. Check the catalog for application restrictions.

If the robot will not uncouple from the tool changer, could the possible cause be that the tool changer requires maintenance?

Yes - consult the product's catalog maintenance section for repair instructions and diagrams. Contact us if the maintenance section that came with your product isn't available.

If the robot will not uncouple from the tool changer, could the possible cause be that there is no air pressure to the tool changer?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air line. 2. Check the condition of the valve connected to the tool changer. 3. Check for valve LEDs during the process. 4. Check the air pressure at the tool changer. 5. Check for leakers, kinks, and breaks in the air lines. 6. Run a program cycle to see whether air comes out of the removed airlines.

If the robot won't couple with the tool changer, could the possible cause an error in the PLC program?

Yes - review the PLC program.

If the robot won't couple with the tool changer, could the possible cause be a broken sensor?

Yes. 1. Check for broken sensor wires. 2. Check that the sensor is plugged into the sensor cable properly.

If the robot won't couple with the tool changer, could the possible cause be a defective valve?

Yes - check to see whether the tool changer can be actuated with a separate shop air line.

If the robot won't couple with the tool changer, could the possible cause be that debris is present in the interface between the robot and the tool changer?

Yes - clean all connecting surfaces, alignment pins, and sensor faces.

If the robot won't couple with the tool changer, could the possible cause be that it's a spring loaded, RQC tool changer?

Yes - check to see whether the tool changer can be actuated with a separate shop air line.

If the robot won't couple with the tool changer, could the possible cause be that the coupling distance is too far?

Yes. 1. Check the coupling position of the robot with respect to the tool half during coupling. The catalog specifies max separation gap distance. 2. Check the lock sensor position.

If the robot won't couple with the tool changer, could the possible cause be that the pressurized air system is contaminated?

Yes. 1. Look for particulate or water in the air lines. 2. Check whether the air filter is clean.

If the robot won't couple with the tool changer, could the possible cause be that the tool changer is broken?

Yes - consult Destaco's customer service for warranty status, repair kits, or Destaco factory repair options.

If the robot won't couple with the tool changer, could the possible cause be that the tool changer mechanism is contaminated?

Yes. 1. Inspect any openings in the tool changer to see whether particulate or debris has entered the tool changer. 2. Check the catalog for application restrictions.

If the robot won't couple with the tool changer, could the possible cause be that the tool changer requires maintenance?

Yes - consult the product's catalog maintenance section for repair instructions and diagrams. Contact us if the maintenance section that came with your product isn't available.

If the robot won't couple with the tool changer, could the possible cause be that there's no air pressure to the tool changer?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air line. 2. Check the valve that is connected to the tool changer. 3. Check for valve LEDs during the process. 4. Check the air pressure at the tool changer. 5. Check for air leaks, kinks, and breaks in the air lines. 6. Run a program cycle to see whether air comes out of the removed airlines.

If the robot won't couple with the tool changer, could the possible cause be too short of an actuation time by the PLC?

Yes - review the PLC program to ensure that the sequencing time doesn't exceed the actuation time mentioned in the slide's manual.

If the tool changer drops the tool during coupling, could the possible cause be an error in the PLC program?

Yes - review the PLC program.

If the tool changer drops the tool during coupling, could the possible cause be that the air lines are reversed?

Yes - switch the air lines going to the tool changer.

If the tool changer drops the tool during coupling, could the possible cause be that the units didn't couple properly?

Yes. 1. Check the pickup position of the robot with respect to the tool during coupling. The catalog specifies the maximum allowed separation gap distance. 2. Check to see whether the lock sensor is installed. (for new units) 3. Check the lock sensor position.

If the tool changer drops the tool during coupling, could the possible cause be that the valve is wired improperly?

Yes - checking the wiring of the valve and the valve's LEDs when sequenced.

If the tool changer drops the tool during normal operation, could the possible cause be errors in the PLC program?

Yes - check the PLC program.

If the tool changer drops the tool during normal operation, could the possible cause be that the PLC program is giving an uncoupled signal out of sequence?

Yes. 1. Check the PLC program. 2. Check the pickup position of the robot with respect to the tool changer during coupling. The catalog specifies the maximum separation distance. 3. The maximum moment load may have been exceeded. 4. The safety spring may be broken. 5. Check the lock sensor's position.

If the tool changer drops the tool during normal operation, could the possible cause be that the valve is wired improperly?

Yes - check the wiring valve and the valve's LEDs when sequenced.

If the tool changer won't actuate, lock, or unlock, could the possible cause be a collision with another object?

Yes - determine whether the robot has crashed into the tooling, causing overload and damage to the tool changer.

If the tool changer won't actuate, lock, or unlock, could the possible cause be a defective valve?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air line. 2. Check the valve for LEDs during the process. 3. Check the air pressure at the tool changer.

If the tool changer won't actuate, lock, or unlock, could the possible cause be a faulty spring failsafe?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air line. 2. Check whether the tool changer returns to its original locked position without use of air.

If the tool changer won't actuate, lock, or unlock, could the possible cause be low air pressure?

Yes. 1. Consult the catalog for minimum air pressure requirements. 2. Check the air pressure at the tool changer. 3. Check for leaks, kinks, and breaks in the air lines.

If the tool changer won't actuate, lock, or unlock, could the possible cause be that the pressurized air system is contaminated?

Yes. 1. Look for particulate or water in the air lines. 2. Check that the air filter is clean.

If the tool changer won't actuate, lock, or unlock, could the possible cause be that the tool changer is broken?

Yes - consult Destaco's customer service for warranty status, repair kits, or Destaco factory repair options.

If the tool changer won't actuate, lock, or unlock, could the possible cause be that the tool changer mechanism is contaminated?

Yes. 1. Inspect any openings in the tool changer to see whether particulate or debris has entered the tool changer. 2. Check the catalog for application restrictions.

If the tool changer won't actuate, lock, or unlock, could the possible cause be that there's no air pressure to the tool changer?

Yes. 1. Check to see whether the tool changer can be actuated with a separate shop air line. 2. Check the valve for LEDs during the process. 3. Check the air pressure at the tool changer. 4. Check for leaks, kinks, and breaks in the air lines. 5. Run a program cycle to see whether air comes out of the removed air lines.

If the tool changer won't actuate, lock, or unlock, could the possible cause be worn seals?

Yes. 1. Remove the air lines from one port and pressurize the other. The seals are worn if air comes out of the open port. 2. Seal kits are available from the accessories section of the main catalog. Most tool changers are field repairable.

Is it OK to mount a smaller tool changer to a robot that has more capability than the tool changer?

No - because a robot can be reprogrammed to do different things than originally intended. This could cause overload and catastrophic failure.

Is there feedback for lock and unlocked positions?

This is determined by the size and type of Tool Changer. Consult the catalog or contact Technical Support.

What are the key features of a tool changer?

The most important features include precise repeatability, high stiffness, high moment carrying capacity and failsafe locking.

What is the air flow requirement, (consumption), for an ARV Venturi?

1.5 SCFM

What makes Robohand tool changers better than the competition?

Our tool changers allow for larger payloads in a smaller package, saving weight and cost.

What sizes are offered for a Double Blank Detector?

Two. 42mm dia. and 54mm dia., and both use a 5in Flatfoot Cup.

What type of utilities are available on tool changers?

Smaller units allow pneumatic and electric connection. Larger units include pneumatic, electric, vacuum, hydraulic, weld gun and servo gun connection.

Cliquez ici pour contacter le service client

En tant qu'entreprise mondialisée, DESTACO compte des représentants de service client dans votre région, où que vous soyez. Contactez le service client DESTACO de votre région pour obtenir une assistance technique, des travaux de réparation, un service sur site et bien plus

ou appelez-nous ()