Processes & Products for Your Automation Applications
The hot stamping process takes lightweight material, hardeneds and strengthens it to form needed shaped parts. Hot Stamping (metal forming, metal stamping), is mostly used in the automotive industry – to form pieces of steel or aluminum into car components/parts. This includes structural components like vehicle doors, frames, hoods, pillars, etc. DESTACO's End Effectors are designed and built to touch, hold and handle the steel and/or aluminum that can be inserted or placed in various types of hot stamping ovens or furnaces, heating the material in excess of 900 degrees C. and also to retrieve the hot stamped parts from the ovens and place them where needed.
Types of Hot Stamping Ovens
There are two types of hot stamping ovens: Soak Oven and Stack Oven. We grab the blank and place in soak oven where conveyor moves part and brings part temp up high, and then our grippers places into a die for stamping. Inside die – runs fluid to cool the item before coming out.
Contact us today to share your project goals and technical specifications with our applications engineers!
 |
AUTOMATING YOUR PRESS ROOM APPLICATIONS
In the Metal Stamping industries, there are common styles of Press Lines that parts are formed on - Progressive, Transfer, Tandem. Progressive Press Lines run smaller parts and do not require automation or tooling to move parts from die to die. Transfer Press Lines have 3 Axis Transfer Rails (Mechinical or Servo) where automation tooling (Finger Tooling) is mounted and used to mtransfer the part from die to die. Transfer Presses have either Mechanical Transfer or Servo Transfer Systems. Mechanical Transfer have a fixed motion relative to the Press Ram timing, where as Servo Transfers motion is not limited to fixed motion, allowing for custom motions of transfer rails to be optimized for maximum throughput. Tandem Line Presses will have multiple Press in a row. In a Tandem Line, there can be between 4 to 7 Presses. The Press tending or part transfer in Tandem lines may have simple 3 Axis Pick and Place Systems or a number of 6 Axis Robots that Load/Unload parts into or out of the presses.
|
AUTOMATION TOOLING & END EFFECTORS
Stamped parts are not always completed parts. Some stampings may need to be welded or assembled to an additional stamping. Metal Assembly is a highly automated part of an automotive plant. Automation Tooling and Robotic End-of-Arm Tooling (EOAT) play a very important role in the success and efficiency of a Metal Assembly Process.
Automation Tooling (aka Finger Tooling) describes the solution utilized in a Transfer Press application to transfer the part. It will consist of a gripper and shovel or some combination of the two. Finger Tooling will include the gripper or shovel back, modular tooling and, the attachment point of a Transfer Rail. The attachment point will have utilities (i.e. Air Supply and Electrical) to operate the Finger Tool.
End effectors (also known as End-of-Arm Tooling, or "EOAT") are devices attached to the end of a robotic arm. They act as the robot’s “hand” and are the portion of the solution that contacts the part being transferred.
|

|
DESTACO provides solutions for all areas of sheet metal forming and automation, including:
For industrial manufacturers who are using robotics in their press shop and body shop operations, it is extremely important that they design and deploy an automation tooling/end-effector system that is compatible with the automation/robotics being used. Below are products DESTACO offers for the sheet metal and automation markets. If our off-the-shelf solutions don't fit, we can produce custom solutions that will. Destaco products designed for your processes include: