DESTACO Introduces Manual Clamp Handle Grips With Multiple Color Options
New innovation is available for use with 14 models within the manual clamp family

DESTACO is excited to announce that the following 14 models in its popular Manual Hand Clamp product family are now available with multiple color options for the clamp handles: 202, 207, 213, 227, 237, 602, 604, 624, 2002, 2007, 2010, 2013, 2017 and 2027.
The new handles are available in five colors: red (standard), black, blue, yellow and green. The new handle colors can be used in almost all industries and applications as a way, for example, to designate specific handles for specialized uses, as part of a safety program, or as a way to create standardized color codes for operating modes or maintenance intervals. The handle colors can also be used as a branding instrument that highlights a company’s corporate color scheme, with customized color designs available.
"Any standard hand-clamp model is interchangeable with a corresponding model that may have a different handle color,” explained Nina Wolleb, Global Application Engineering Manager for DESTACO. "Upon request, these handle colors can also be made available for other DESTACO product lines, such as UB hand-clamp versions or locking clamps. Be aware, though, that at this time, these special handle colors are not available for use with dipped T-handles."
To learn more about any of DESTACO’s high-performance automation, workholding or remote-handling solutions, please visit destaco.com or call (888) DESTACO (888-337-8226).